NXP Semiconductors


Select site:

English

PCA9633

Selection guide

Datasheet

PCA9633
(Product Specification)
25-Jul-08, 43 pages, 228 kB

Download all documentation

General description

The PCA9633 is an I2C-bus controlled 4-bit LED driver optimized for Red/Green/Blue/Amber (RGBA) color mixing applications. Each LED output has its own 8-bit resolution (256 steps) fixed frequency Individual PWM controller that operates at 97 kHz with a duty cycle that is adjustable from 0 pct to 99.6 pct to allow the LED to be set to a specific brightness value. A fifth 8-bit resolution (256 steps) Group PWM controller has both a fixed frequency of 190 Hz and an adjustable frequency between 24 Hz to once every 10.73 seconds with a duty cycle that is adjustable from 0 pct to 99.6 pct that is used to either dim or blink all LEDs with the same value.

Each LED output can be off, on (no PWM control), set at its Individual PWM controller value or at both Individual and Group PWM controller values. The LED output driver is programmed to be either open-drain with a 25 mA current sink capability at 5 V or totem pole with a 25 mA sink, 10 mA source capability at 5 V. The PCA9633 operates with a supply voltage range of 2.3 V to 5.5 V and the outputs are 5.5 V tolerant. LEDs can be directly connected to the LED output (up to 25 mA, 5.5 V) or controlled with external drivers and a minimum amount of discrete components for larger current or higher voltage LEDs.

The PCA9633 is one of the first LED controller devices in a new Fast-mode Plus (Fm+) family. Fm+ devices offer higher frequency (up to 1 MHz) and more densely populated bus operation (up to 4000 pF).

The active LOW Output Enable input pin (OE) allows asynchronous control of the LED outputs and can be used to set all the outputs to a defined I2C-bus programmable logic state. The OE can also be used to externally PWM the outputs, which is useful when multiple devices need to be dimmed or blinked together using software control. This feature is available for the 16-pin version only.

Software programmable LED Group and three Sub Call I2C addresses allow all or defined groups of PCA9633 devices to respond to a common I2C address, allowing for example, all red LEDs to be turned on or off at the same time or marquee chasing effect, thus minimizing I2C-bus commands.

The PCA9633 is offered with 3 different I2C-bus address options: fixed I2C-bus address (8-pin version), 4 different I2C-bus addresses from 2 programmable address pins (10-pin version), and 126 different I2C-bus addresses from 7 programmable address pins (16-pin version). They are software identical except for the different number of address combinations.

The Software Reset (SWRST) Call allows the master to perform a reset of the PCA9633 through the I2C-bus, identical to the Power-On Reset (POR) that initializes the registers to their default state causing the outputs to be set HIGH (LED off). This allows an easy and quick way to reconfigure all device registers to the same condition.

Features

  • 4 LED drivers. Each output programmable at:
    • Off
    • On
    • Programmable LED brightness
    • Programmable group dimming/blinking mixed with individual LED brightness
  • 1 MHz Fast-mode Plus I2C-bus interface with 30 mA high drive capability on SDA output for driving high capacitive buses
  • 256-step (8-bit) linear programmable brightness per LED output varying from fully off (default) to maximum brightness using a 97 kHz PWM signal
  • 256-step group brightness control allows general dimming (using a 190 Hz PWM signal) from fully off to maximum brightness (default)
  • 256-step group blinking with frequency programmable from 24 Hz to 10.73 s and duty cycle from 0 pct to 99.6 pct
  • Four totem pole outputs (sink 25 mA and source 10 mA at 5 V) with software programmable open-drain LED outputs selection (default at totem pole). No input function.
  • Output state change programmable on the Acknowledge or the STOP Command to update outputs byte-by-byte or all at the same time (default to 'Change on STOP').
  • Active LOW Output Enable (OE) input pin. LED outputs programmable to '1', '0' or 'high-impedance' (default at power-up) when OE is HIGH, thus allowing hardware blinking and dimming of the LEDs (16-pin version only).
  • 2 hardware address pins (10-pin version) and 7 hardware address pins (16-pin version) allow respectively up to 4 and 126 devices to be connected to the same I2C-bus. No hardware address pins in the 8-pin version.
  • 4 software programmable I2C-bus addresses (one LED Group Call address and three LED Sub Call addresses) allow groups of devices to be addressed at the same time in any combination (for example, one register used for 'All Call' so that all the PCA9633s on the I2C-bus can be addressed at the same time and the second register used for three different addresses so that 1/3 of all devices on the bus can be addressed at the same time in a group). Software enable and disable for I2C-bus address.
  • Software Reset feature (SWRST Call) allows the device to be reset through the I2C-bus
  • 25 MHz internal oscillator requires no external components
  • Internal power-on reset
  • Noise filter on SDA/SCL inputs
  • Edge rate control on outputs
  • No glitch on power-up
  • Supports hot insertion
  • Low standby current
  • Operating power supply voltage range of 2.3 V to 5.5 V
  • 5.5 V tolerant inputs
  • -40 Cel to +85 Cel operation
  • ESD protection exceeds 2000 V HBM per JESD22-A114, 200 V MM per JESD22-A115, and 1000 V CDM per JESD22-C101
  • Latch-up testing is done to JEDEC Standard JESD78 which exceeds 100 mA
  • Packages offered: SO, TSSOP (MSOP), HVQFN, HVSON

Products/packages

Type numberNorth American Type numberOrdering code (12NC)Product statusPackagePackingMarkingChemical contentLeadfree conversion date
PCA9633BSPCA9633BS-T9352 813 08118Volume productionSOT629-1
(HVQFN16)
Reel Pack, SMD, 13"Standard MarkingPCA9633BS
Always Pb-free
PCA9633D16PCA9633D169352 813 09112Volume productionSOT109-1
(SO16)
TubeStandard MarkingPCA9633D16
Always Pb-free
PCA9633D16PCA9633D16-T9352 813 09118Volume productionSOT109-1
(SO16)
Reel Pack, SMD, 13"Standard MarkingPCA9633D16
Always Pb-free
PCA9633DP1PCA9633DP1-T9352 813 12118Volume productionSOT505-1
(TSSOP8)
Reel Pack, SMD, 13"Standard MarkingPCA9633DP1
Always Pb-free
PCA9633DP2PCA9633DP2-T9352 813 13118Volume productionSOT552-1
(TSSOP10)
Reel Pack, SMD, 13"Standard MarkingPCA9633DP2
Always Pb-free
PCA9633PWPCA9633PW9352 814 16112Volume productionSOT403-1
(TSSOP16)
TubeStandard MarkingPCA9633PW
Always Pb-free
PCA9633PWPCA9633PW-T9352 814 16118Volume productionSOT403-1
(TSSOP16)
Reel Pack, SMD, 13"Standard MarkingPCA9633PW
Always Pb-free
PCA9633TKPCA9633TK-T9352 816 18118Volume productionSOT908-1
(HVSON8)
Reel Pack, SMD, 13"Standard MarkingPCA9633TK
Always Pb-free

Pricing/ordering/availability

Type numberOrdering code(12NC)Indicative price/unit($)RegionDistributorIn stockOrder quantityInventory dateBuy onlineSamples
PCA9633BS9352 813 08118  1.0400NADIGI-KEY CORPORATION6,000 1/6/2009Buy onlineOrder samples
   NADIGI-KEY CORPORATION8,759 1/6/2009Buy online 
PCA9633D169352 813 09112  1.0400NAAVNET ELECTRONICS MARKETING995 1/7/2009Buy onlinenot available
   NADIGI-KEY CORPORATION146 1/6/2009Buy online 
PCA9633D169352 813 09118  1.0400NAMOUSER ELECTRONICS2,375 1/7/2009Buy onlineOrder samples
PCA9633DP19352 813 12118  1.0400NADIGI-KEY CORPORATION5,000 1/6/2009Buy onlineOrder samples
   NADIGI-KEY CORPORATION5,585 1/6/2009Buy online 
   NAMOUSER ELECTRONICS2,236 1/7/2009Buy online 
PCA9633DP29352 813 13118  1.0400NADIGI-KEY CORPORATION7,500 1/6/2009Buy onlineOrder samples
   NADIGI-KEY CORPORATION9,372 1/6/2009Buy online 
   NAFUTURE ELECTRONICS3,000 1/7/2009Buy online 
   NAMOUSER ELECTRONICS170 1/7/2009Buy online 
PCA9633PW9352 814 16112  1.0400NADIGI-KEY CORPORATION2,130 1/6/2009Buy onlinenot available
PCA9633PW9352 814 16118  1.0400NAMOUSER ELECTRONICS2,459 1/7/2009Buy onlineOrder samples
PCA9633TK9352 816 18118  0.9300      Order samples

Block diagrams/pinning

Parametrics/similar products

Type numberPackageEnableOperating
temp.(Cel)
PWMsI²C-bus
interface
# of BitsI²C-bus(kHz)Operating voltage(VDC)Max Sink Current per bit(mA)# of AddressesMax Sink Current
per package(mA)
PCA9633BSSOT629-1
(HVQFN16)
yes-40~855 (4 x 97 kHz dim and 1 x 97 kHz dim or 24 Hz to 10.73 sec blink)Fast Mode Plus 30 mA SDA outputs for 4000 pF bus410002.3~5.525126100
PCA9633D16SOT109-1
(SO16)
yes-40~855 (4 x 97 kHz dim and 1 x 97 kHz dim or 24 Hz to 10.73 sec blink)Fast Mode Plus 30 mA SDA outputs for 4000 pF bus410002.3~5.525126100
PCA9633DP1SOT505-1
(TSSOP8)
no-40~855 (4 x 97 kHz dim and 1 x 97 kHz dim or 24 Hz to 10.73 sec blink)Fast Mode Plus 30 mA SDA outputs for 4000 pF bus410002.3~5.5251100
PCA9633DP2SOT552-1
(TSSOP10)
no-40~855 (4 x 97 kHz dim and 1 x 97 kHz dim or 24 Hz to 10.73 sec blink)Fast Mode Plus 30 mA SDA outputs for 4000 pF bus410002.3~5.5254100
PCA9633PWSOT403-1
(TSSOP16)
yes-40~855 (4 x 97 kHz dim and 1 x 97 kHz dim or 24 Hz to 10.73 sec blink)Fast Mode Plus 30 mA SDA outputs for 4000 pF bus410002.3~5.525126100
PCA9633TKSOT908-1
(HVSON8)
no-40~855 (4 x 97 kHz dim and 1 x 97 kHz dim or 24 Hz to 10.73 sec blink)Fast Mode Plus 30 mA SDA outputs for 4000 pF bus410002.3~5.5251100


Similar products
PCA9633 links to the similar products page containing an overview of products that are similar in function or related to the type number(s) as listed on this page. The similar products page includes products from the same catalog tree(s), relevant selection guides and products from the same functional category.

Disclaimer

The information published on product information pages of the www.nxp.com or www.semiconductors.com websites is an extract from product data sheets and is for information purposes only. For detailed information please check the most recent version of the relevant product data sheet as published on these websites. In the event of any conflict between product information pages and data sheets or deviations from information provided in the product data sheets on these product information pages, the information provided in the product data sheets shall prevail.


The product status of the product(s) described in the product data sheet may have changed since publication of the data sheet and therefore information in datasheets on product status may be outdated. The latest information on product status is published on the product information pages of the above-mentioned websites.


As from October 1st, 2006 Philips Semiconductors has a new trade name - NXP Semiconductors, which will be used in future data sheets together with new contact details. In data sheets where the previous Philips references remain, please use the new links as shown below.


http://www.philips.semiconductors.com use http://www.nxp.com
http://www.semiconductors.philips.com use http://www.nxp.com (Internet)
sales.addresses@www.semiconductors.philips.com use salesaddresses@nxp.com (e-mail)

The copyright notice at the bottom of each page (or elsewhere in the document, depending on the version)
- © Koninklijke Philips Electronics N.V. (year). All rights reserved -
is replaced with:
- © NXP B.V. (year). All rights reserved.-


If you have any questions related to the data sheet, please contact our nearest sales office via e-mail or phone (details via salesaddresses@nxp.com). Thank you for your cooperation and understanding.